AXIS#.VL.AINSCALE
Description
AXIS#.VL.AINSCALE is an analog velocity scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 1 (analog velocity mode).
The value entered is the motor velocity per 1 V of analog input. This value may be either higher or lower than the application velocity limit (AXIS#.VL.LIMITP orAXIS#.VL.LIMITN ), but the actual analog I/O will be limited by AXIS#.VL.LIMITP or AXIS#.VL.LIMITN .
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
General Information
Type |
Read/Write |
Units |
Rotary: RPM See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
0 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.VL.AINSCALE | 0x5011 | 0x9 | UDINT | 1000:1 | - | RW | False |
AXIS2.VL.AINSCALE | 0x5111 | 0x9 | UDINT | 1000:1 | - | RW | False |